Industry Online Support
Technical Forum
10/22/2011 5:28 PM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181)
|
Hello, Anyway to take a backup from TP177 micro: 1. Prosave 2. RS232/PPI Multi-Master- cable (6ES7901-3CB30-0XA0).The RS232/PPI Multi Master cable (with 8 DIP switches) can be used if DIP switch number 5 is set to PPI/freeport ("0"). The cable must be dead for it to accept the change. Or USB/PPI cable 6ES7 901-3DB30-0XA0 can be used for downloading since WinCC flexible 2005 SP1! Follow this How do you backup/restore with a Windows-based panel? best regards, Hristo Mihalev |
10/23/2011 4:59 AM | |
Posts: 6 Rating: (0) |
hi will it work if i create a back up of a tp 170 micro(the old device) and restore it on a tp 177 micro???
|
10/26/2011 3:15 PM | |
Posts: 6 Rating: (0) |
thats what i already wanted to do but the problem is that the old one is a tp 170 micro and the new one is a tp 177 micro. |
10/27/2011 9:10 AM | |
Posts: 3037 Rating: (192)
|
Hello, Then, you need the project of this TP170 micro. The backup of the TP170 micro to a restore to TP177 micro does not work. Tweety |
Follow us on