Industry Online Support
Technical Forum
10/4/2011 5:48 PM | |
Posts: 19 Rating:
|
I have some problems with setting up two stations, Station-2 as an I-Device where I generated a GSD-file, that then is attached to the Station-1 ProfiNET system. I have attached the 2 stations hardware config files, and also the GSD-file that I generated from Station-2. The problem is that Station-1 can't seem to find Station-2. I'm struggling with a big question, * Is the IP-adress for station-2 automatically generated into the GSD-file and that I don't have to give station-1 these adress parametres for station-2? AttachmentHardwareConf.zip (111 Downloads) |
Follow us on