5/1/2017 11:09 AM | |
Posts: 8 Rating: (0) |
Good afternoon! I have a big problem during installation Step 7. I try to install STEP 7 Professional 2006 SR4 on Oracle VM Virtualbox (Windows 7 Enterprise SP1 Original ISO Updated 2014.09 (x86-x64) [Ru]). The Antivirus programm is not installed, firewall is switched off. There is a message during installation Step 7 : The wizard was interrupted before Step 7 could be completely installed. Your system has not been modified. To complete installation at another time , please run setup again. I tryed to run setup again, restart Windows - the same problem. What should i do? Where is my fault? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/3/2017 2:27:00 PMNew subject after splitting |
|
5/1/2017 2:32 PM | |
Joined: 11/16/2006 Last visit: 8/5/2024 Posts: 92 Rating: (15) |
STEP 7 Professional 2006 SR4 = STEP 7 V5.4 incl. SP3.1 not work with Windows 7 https://support.industry.siemens.com/cs/document/27460215/step-7-professional-2006-service-release-4
with Windows 7 use STEP 7 Professional 2010 SR4
|
This contribution was helpful to1 thankful Users |
Follow us on