5/10/2019 7:05 PM | |
Posts: 15 Rating: (0) |
Hi all I created a test website with the LWE. The red switch in the figure changes the value of the variable V1.0 to "1", and that state should be seen showing an "M" motor figure. When the variable V1.0 changes to "0" through the NI1 -- NQ1 input/output, it should be reflected showing the red disk. The problem is that the variable V1.0 is activated to "1", it works fine, but this change is not reflected in the web. I created a disconnection delay to keep the status "1" for a while, in case the cause was a delay in the transmission of data, but it does not work either. Any ideas? AttachmentLWE.zip (161 Downloads) |
5/10/2019 7:56 PM | |
Posts: 15 Rating: (0) |
I reduced the web, and I have leave only the button. The program run correctly, but I no see changes in the image. AttachmentLOGO_WEB_EDITOR.zip (175 Downloads) |
5/10/2019 8:39 PM | |
Posts: 15 Rating: (0) |
Thanks! Really, the output Q1 is only set in the program for checking. With this program, what I try is to make the pushbutton function, but the problem is that in LWE the button does not update the image changes that should correspond to the states "1" or "0" in the web. I have set the delay of 2 seconds to maintain the status "1" in case the problem of not updating the images was due to a delay in the communication between the PLC and the web. Attachmentpush_button_LOGO_WEB_EDITOR2.zip (167 Downloads) |
5/10/2019 8:44 PM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
Is your problem now solved with the suggestion from me? If so, please mark the topic as solved. |
5/10/2019 9:23 PM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
I still do not understand your actual problem after your last statement. What do you want to do? |
Follow us on