8/9/2010 11:24 AM | |
Joined: 1/4/2007 Last visit: 5/28/2024 Posts: 1127 Rating: (174)
|
Hello Franco U. See also the chapter 8.2 of the Siwarex MS manual. You can find the Siwarex MS manual on the internet: http://support.automation.siemens.com/WW/view/en/22600601 3. Is the parameter “FirstVB_POINTER” of the library “MicroScale_V20” and the library “MicroScale_additional” the same? 4. Which parameters do you mean exactly with “…I've seen that the byte that should tell me wich command has been given doesn't change its status”? 5. What do you mean with:”I mean giving a trigger by PC and by PLC (using status table) should be same, right?”? If you are triggering a command via Siwatool, you’ll see no changing of the parameters into the Step7-program. There is no problem with the library. Best regards Siwarexi |
Follow us on