6/20/2015 4:39 PM | |
Joined: 10/20/2009 Last visit: 4/3/2017 Posts: 215 Rating:
|
Dear All, The PCS7 version i am using is PCS7 V7.1 SP4 I am using Security Scalance S623 to establish communication between DMZ Zone and Internal Zone. I have OpenPCS7 station in DMZ zone and OS Server in Internal Zone. I have set the firewall rules to access these two PCs i.e. OS Server and OpenPCS7. I am able to ping and i am able to share the folders in between these two PC's. But when i open OPC Scout as client on OpenPCS7 machine and try to access the OS Server. I get the error as attached here. Also i have attached the OPC Scout Log as well. Can anyone tell me, why i am getting this error? What kind of settings we need to do for Firewall to get access the OS server? Please help. AttachmentOPC Error Log and Config.zip (108 Downloads) |
Regards, |
|
Follow us on