8/23/2013 2:48 PM | |
Joined: 9/27/2007 Last visit: 10/4/2024 Posts: 2 Rating: (0) |
Dear all, I have similiar problem with PC7 V7.0 SP3 on operating system win XP SP2 pro en. I have 3 AS, 1 ES, 3 OS.All OS and ES are same configuration,One of AS is redundant the others are normal CPU. When I open WINCC runtime I saw not active on the top of WINCC.No butons active that coming from plant hierercy.So I made OS compile ( changes only ) run one time os project editor.And then uninstall WINCC and install again. WINCC shows redundant CPU tags but the others AS no informaiton comes. And the I download only connections and gateways.I couldn't solve problem. Can anybody help me? Attachmentprintscreen.zip (88 Downloads) |
Last edited by: O_Moderator at: 8/26/2013 11:04 AMLast edited by: O_Moderator at: 8/26/2013 11:03 AMnew subject after splitting from /tf/WW/en/Posts/83786#top Last edited by: surmanset at: 8/23/2013 11:01 PM |
|
3/7/2014 9:50 PM | |
Posts: 37 Rating: (2)
|
Hello , PCS 7 SP3 is not supported on XP SP2 only XP SP3 I woulld recommd that you upgrade to XP SP3 and retest |
This contribution was helpful to1 thankful Users |
7/30/2020 7:42 PM | |
Joined: 5/18/2020 Last visit: 1/6/2024 Posts: 2 Rating: (0) |
How your problem gets rectified as I am facing same problem? Please give some advice. |
Follow us on