Industry Online Support
Technical Forum
2/13/2014 1:16 PM | |
Joined: 1/25/2006 Last visit: 2/9/2023 Posts: 257 Rating: (60) |
Hello, I used aplication example set 22 (data communication S7 1200 with PAC3200 via Modbus TCP). Hardware: S7 1200 and 7 PAC3200s. When I start program, from 4 PACs I read everything, but from 3 PACs nothing. I check program and I thing that is OK. What I notice when I analized PACs DB ( from one which I can read data and one where I can't read). Exception error in TRUE on PAC from which I can't read data. Can someone tell me what's happened and how to solve it? In attach you can see some parameters from 'good' and 'bad' PAC
AttachmentPAC3200.zip (121 Downloads) |
Follow us on