4/14/2023 6:26 AM | |
Joined: 1/21/2013 Last visit: 10/14/2024 Posts: 3176 Rating: (492) |
Hi MMS12, I would try to load the latest firmware to get the PLC working again. It is quite understandable - and not uncommon - to try a quick reset in the event of an error. However, as you may have noticed, in some cases the contents of the diagnostic buffer are lost. So a tip from me is to save the diagnostic buffer first and then try a reset. Kind regards |
Follow us on