11/22/2017 8:28 AM | |
Posts: 44 Rating: (0) |
Hello I have problem with uploading program from CPU S7-200 When I want to upload , I receive the error that is shown in attached file . In the attached file , there are 2 pictures related to PLC & PC adapter status and another one is the error . I set in "PG/PC Interface " : PC ADAPTER PPI How should I solve it ? Thanks. AttachmentDoc1.pdf (113 Downloads) |
Last edited by: hossein82 at: 11/22/2017 8:29:23 AM |
|
Follow us on