4/1/2009 12:34 PM | |
Joined: 9/27/2006 Last visit: 7/3/2024 Posts: 12266 Rating:
|
Babelfish translation : How do you do. Alexander seems to be refering to a Fujitsu Esprimo PC, model 5545:There are F/S esprimo mobile v5545, Step 7 v5.4 sp1. F/S has built-in USB-reader. MMC of strange producer with the load into the device are defined as Flash of device. MMC of 512k 6ES7953-8LJ11-0AA0 is not determined. Reading through INT13h occurs without the errors - accessible completely. " Memory of card of parametr of assignment" does not support USB- interface. There can be I something I do not know? It is very small in the Russian language (although the delivery into Russia implies the russification of product) of information, transfers are not always correct. It turns out that claim about the standardization and about the openness of the system only of word? Thanks, with respect Alexander. http://sp.ts.fujitsu.com/dmsp/docs/ds_esprimo_mobile_v5545.pdf There is a USB card reader on-board, and he seems to have problems accessing a Siemens MMC card with it. Anybody (else) can help? Daniel Chartier |
4/2/2009 9:24 AM | |
Joined: 4/24/2006 Last visit: 7/3/2024 Posts: 8708 Rating:
|
Dear Alexander, I have to admit, my Russian is very bad Thanks to Daniel, I will try to answer. Please have a look at the following links: http://support.automation.siemens.com/WW/view/en/21829579 http://support.automation.siemens.com/WW/view/en/21831257 http://support.automation.siemens.com/WW/view/en/21830727 So you need a USB prommer to read and write MMC I hope it might help you. Best regards, Wizard |
Follow us on