5/22/2012 7:44 AM | |
Joined: 8/25/2006 Last visit: 9/12/2024 Posts: 2209 Rating: (278) |
Hello. Via which interface you tried to change parameters (G-SST1, G-SST2 or G-SST3)? Check this and enable parametrization for required interface in P927. Parameters differ in length (word/double-word) and in index/non-index (array/non-array), so you must send different requests to change different parameters, have a look at themanualabout different types of requests, chapter 7.7.9.
|
8/31/2012 7:14 PM | |
Joined: 8/25/2006 Last visit: 9/12/2024 Posts: 2209 Rating: (278) |
[quote user="kb8vsa"]SO ,.. should you are suggesting that P927 sould also have SST 2 turned on ? Yes, of course. |
9/1/2012 6:00 AM | |
Joined: 8/25/2006 Last visit: 9/12/2024 Posts: 2209 Rating: (278) |
As I understood, now after properly setting of P927 you could change any non-indexed parameter, but could not change parameter with index. You should send another request to change parameter with index. Try to read againmanualabout different types of requests, chapter 7.7.9, that I suggested you earlier. |
Follow us on