11/14/2024 1:30 PM | |
Joined: 2/5/2021 Last visit: 11/19/2024 Posts: 30 Rating: (0) |
Hello, I generate file for WinCC runtime but when I start runtime it doesn't have connection with PLC. I can connect with TIA portal to PLC without problem. When I transfer WinCC Runtime to other PC and int TIA portal in PC Station change PC name to the name of that PC it works without problem. I follow this instructions What should you watch out for when downloading WinCC Runtime Professional from the... - ID: 88780011 - Industry Support Siemens I tried everything, change order on network adapter setting, SIMATIC Shell is OK, PC name is OK, adapter settings are OK, SQL server is running, I even try uninstall WinCC Runtime and SQL server but it didn't help, I am administrator on this PC. I have 2 network card. On Integrated network card I am connected to my work network and with USB network card I am connected directly to PLC. Someone have some recommendations? Thank you |
Last edited by: Moderator_Lan at: 11/14/2024 13:31:56link optimized |
|
Follow us on