9/2/2021 2:41 PM | |
Joined: 8/21/2021 Last visit: 4/22/2022 Posts: 4 Rating: (0) |
i am installing pcs7 v9.1 I have problem with windows 10 enterprise LTSC 2019 Build 17763.2114 please help me! ------------------------------------------------------------------------------------------ |
Last edited by: dunghuuhaha at: 09/02/2021 15:22:19Last edited by: The Helping Hand at: 09/03/2021 07:05:50New subject after splitting |
|
9/3/2021 6:59 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Looks something is wrong with your Windows installation. cmd is the command prompt. Can you check if that works? Right click the Windows symbol on the taskbar->Run and enter: cmd and press OK |
If I could help you, you can use the RATE button. Thank you. |
|
9/4/2021 11:41 AM | |
Joined: 8/21/2021 Last visit: 4/22/2022 Posts: 4 Rating: (0) |
i checked but cmd is working properly. Thank you for your interest |
Last edited by: dunghuuhaha at: 09/04/2021 11:42:55 |
|
9/5/2021 9:42 AM | |
Joined: 8/21/2021 Last visit: 4/22/2022 Posts: 4 Rating: (0) |
Thank you for your interest I have tried and can't fix this error. |
9/9/2021 6:49 AM | |
Posts: 198 Rating: (60) |
Hello, Is your Windows updated with the latest patches? Are you getting this error only in one of your installations or all of them? |
9/17/2021 5:31 AM | |
Joined: 8/21/2021 Last visit: 4/22/2022 Posts: 4 Rating: (0) |
i have updated all windows 10 ltsc updates and installed pcs7 v9.1 |
9/17/2021 6:27 AM | |
Joined: 1/11/2019 Last visit: 4/23/2024 Posts: 684 Rating: (139) |
Great! |
3/29/2024 7:49 AM | |
Joined: 7/13/2023 Last visit: 4/23/2024 Posts: 2 Rating: (0) |
I have similar problems and Win server 2019. Do you have any ideas yet? |
Follow us on