Industry Online Support
Technical Forum
7/6/2010 6:25 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477)
|
P100=3 means Sensor Less Vector control and P100=1 V/F mode... In V/F, drive will run motor on constant V/F ratio.. But when you talk about Vector Control, Speed controller and Current controller will come in Picture.. You have to perform Auto tunning.. Have you did this?? For this, Set P115 = 2, 4 and then 5 Refer Compendium for More Details, Regards, Devesh Vithani |
Last edited by: Vithani at: 7/8/2010 6:52 PMLast edited by: Vithani at: 7/8/2010 6:49 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
7/13/2010 5:32 PM | |
Posts: 13 Rating: (0) |
thanks mr vithani problem is solved as per ur instruction....thanks from narinder & pravin |
This contribution was helpful to1 thankful Users |
Follow us on