9/28/2018 9:25 AM | |
Posts: 6 Rating: (0) |
Hello there, I got Problems by connecting the iot2040 with my Computer. I tried to connect them with Ethernet (eth0 / X1P1). When I tried to ping the static address 192.168.200.1 with cmd there was no answer or the Connection timed out. I set the Address of my PC on 192.168.200.99. And they are in the same Subnet. (255.255.255.0) I also deaktivated my Firewall and used other LAN cable. Still no answer. Then I tried to connect with the eth1 and DHCP. In both cases the green and the yellow LED was lighting, but still no Connection. ------------------------------------------------------------------------------------------ |
Last edited by: Flach at: 9/28/2018 9:28:14 AMLast edited by: Flach at: 9/28/2018 11:16:42 AMLast edited by: The Helping Hand at: 9/28/2018 11:17:42 AMNew subject after splitting |
|