4/27/2021 5:44 PM | |
Joined: 7/14/2017 Last visit: 4/4/2022 Posts: 33 Rating:
|
Hello! I am using a IoT2050 Advanced device with IOT2050_Example_Image_V1.0.2.img running in the SD card. I have installed a SIMCom 7600E-H modem in the mPCIe (https://techship.com/products/simcom-sim7600e-h-lte-cat-4-mpcie-sim/) and I have added a SIM card with 4G communication (Euskaltel company). I am trying to get connected to the Internet using the steps from "SIMATIC IOT2050 - Modem via mPCIe" PDF. This is the result for the commands: [snip] What's the problem? The SIM card hasn't got PIN number. Does anyone know what is giving me that issue? Thanks! AttachmentResult_Commands.txt (192 Downloads) |
Last edited by: Jen_Moderator at: 04/28/2021 12:11:21Added result of commands as a txt. file. |
|
4/28/2021 9:52 AM | |
Joined: 12/12/2016 Last visit: 11/27/2023 Posts: 640 Rating:
|
Hello, Could you provide us also the outputs of these commands?
Best Regards! |
4/28/2021 10:15 AM | |
Joined: 7/14/2017 Last visit: 4/4/2022 Posts: 33 Rating:
|
Hi! First of all, thanks for your reply. [snip] What it concerns me is that sometimes some minutes after reboot, mmcli -L command shows "No modems were found" AttachmentOutput_Commands.txt (175 Downloads) |
Last edited by: Jen_Moderator at: 04/28/2021 12:12:34Added output as txt file. |
|
4/29/2021 1:01 PM | |
Joined: 12/12/2016 Last visit: 11/27/2023 Posts: 640 Rating:
|
Hello, based on the outputs it appears the card is recognized correctly on the usb bus at first, but its suspicious that the ModemManager claims it invalid after a while. Could either be a problem with missing drivers or the card itself. Do you have the possibility to test this card in a Laptop? have you connected an Antenna when installing in the IOT. One further command you could check is:
To see if necessary drivers could be loaded. On my HUAWEI Card which is working the output looks looks like this (check attachment) Best Regards! Attachmentusb-devices_output.txt (191 Downloads) |
Last edited by: Fe_lipe at: 04/29/2021 13:04:51Last edited by: Fe_lipe at: 04/29/2021 13:06:37added attachment |
|
Follow us on