5/5/2021 1:52 PM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, seems that it gets stuck at stopping Regular background program". I don't know if this is related or the same problem, but there was an issue existing on github regarding a failed reboot. I also wonder about the different outputs in your two logs. E.g. in the working example, there is no Stopping tcf-agent or Stopping Mosquitto. Is it possible for you to try to build the current master branch from github and see if this problem still exists? Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
5/6/2021 12:53 PM | |
Joined: 7/14/2017 Last visit: 4/4/2022 Posts: 33 Rating: (0) |
Hello, I have installed the current master branch from Github. I will write again if the problem persists. Thanks! |
Follow us on