11/23/2009 12:30 AM | |
Joined: 10/7/2005 Last visit: 8/7/2024 Posts: 3016 Rating:
|
Hello pido if you replace the CPU with an indentical oneyou will not need to re-program the EPROM. I am however worried that your said "it worked for two or three minutes" and wonder if there is something else wrong that leads to the CPU fault (which means a new CPU may not last long either). Should you need more help, it would help us to help you if yougive us some more details about your S5 system (e.g. part numbers, system configuration etc.) and the fault that you observed (which LED's are ON,OFF and/or flashing). I hope this helps for now. |
Cheers |
|
Follow us on