3/15/2016 2:21 PM | |
Joined: 7/9/2015 Last visit: 12/1/2023 Posts: 3606 Rating:
|
Hi, are the software versions of the installed software really the same? I saw, that you have an older version of F-Configuration Pack. Now its V5.5 + SP12 https://support.industry.siemens.com/cs/ww/de/view/15208817 You could also do a repair installation of your S7 V5.5 SP4. Regards, Towome |
If my post was useful, please rate me - thank you! |
|
3/16/2016 7:31 AM | |
Joined: 4/27/2011 Last visit: 10/19/2023 Posts: 13 Rating:
|
Yes, software versions are the same. I just reinstalled Step7 and safety sofware and it's still the same. Strange is I have problems only with Hardware compilation, but if I compile hardware of this project from another PC I can compile safety software. The fault I'm getting has number 1129:2076 Can anybody tell me what it comes from? PS. I found a solution. with help to related topic (link below), I changed language settings decimal char coma->dot and I now can compile safety hardware Dear Siemens, is it a bug, or there's any reason for this? detail description of solution in this topic: https://support.industry.siemens.com/tf/ww/en/posts/error-message-1129-2076-internal-consistency-check-of-the-resource-failed/120679/?page=0&pageSize=10#post581070 |
Last edited by: bartoszbb at: 3/16/2016 7:56:24 AMLast edited by: bartoszbb at: 3/16/2016 8:06:35 AMLast edited by: bartoszbb at: 3/16/2016 8:07:43 AM |
|
Follow us on