8/18/2023 7:10 AM | |
Joined: 5/30/2022 Last visit: 12/20/2024 Posts: 610 Rating: (99) |
Hi TF_DongDong, Unified and Professional cannot be installed on the same PC due to incompatibility between databases, you can only have one, if you want to have both I recommend using a virtual machine, anyway, if you want to uninstall Professional correctly, review the following information: Installation error of WinCC Unified PC RT with WinCC Professional |
If this information really helps, you could use the Rate function. |
|
8/18/2023 8:49 AM | |
Joined: 5/21/2020 Last visit: 2/27/2024 Posts: 6 Rating: (0) |
Thank you for your answer. I have already tried the solution you suggested in "Installation error of WinCC Unified PC RT with WinCC Professional", "How do you uninstall a SIMATIC WinCC Professional or a SIMATIC WinCC Runtime Professional SQL Server Instance?", but I am getting the same error. |
Follow us on