Industry Online Support
Technical Forum
10/9/2013 9:29 AM | |
Joined: 10/7/2005 Last visit: 9/18/2024 Posts: 3021 Rating: (1054)
|
Hello chikhim you are using MW 2 as the index value but increment it by 2 which I presumeyou doto cater for the word based (or 16 bit based) addressing in the DB (which will have a bunch ofInteger values in it judging by your logic). This conflicts though with how you create the pointer value which you do viaa "SLD 4" which also caters for word based addressing ("SLD 3" is what you typically use to create an S7 pointer value). I suggest you either change the way you handle MW2 OR the way you create the pointer value (the same applies too for the way you handle MW 70). I hope this helps and have a look to at Information on the topic of "Indirect addressing" for moreon this. |
Cheers |
|
Follow us on