9/1/2014 1:18 PM | |
Joined: 10/7/2005 Last visit: 11/1/2024 Posts: 3025 Rating: (1055)
|
Hello Lee T port mirroring can unfortunately put quite a burden on your switch and lead to performance loss and drop of packets, which is something safety related messages don't take to lightly too (in other words, it can explain why your distributed safety network goes down once you enable port mirroring). Ethernet/IP (which some call a desease rather than a protocol) is traditionallyUDP and Multicast based and mirroring its traffic may very well be the straw that breaks theCamel's back in this case once you enable port mirroring. You unfortunetly are kind ofstuck in Heisenbergs uncertainty principle (i.e. your attempt to monitor things influences the realibility of your measurement). Apart from removing the Ethernet/IP traffic from the Network (I agree with Marko Bursicthat it has no business there), I'd also suggest you use a Network Tap (e.g. ProfiTap, located at your S7 PN port) instead of using port mirroring to analyse your Network, as a Tap does not suffer from the issues that affects port mirroring. I hope this helps and please let us know what you find. |
Cheers |
|
Follow us on