6/6/2024 5:25 AM | |
Joined: 9/3/2008 Last visit: 6/26/2024 Posts: 926 Rating:
|
Hi Roulik, As for the remote access, please review the following FAQ: Remote access to WinCC stations For a WinCC Rumtime system with several users, you would need a server/client system if they need access at the same time. So you need a WinCC server and x number of clients. About "Security Controller", then yes, you need to stop the runtime and start the security controller and press repeat settings and after that, restart Windows. Best regards Michael |
Michael |
|
This contribution was helpful to
1 thankful Users |
Follow us on