7/23/2019 5:44 PM | |
Posts: 9 Rating: (0) |
According to the sensor manual, I just connect the lines in yellow. And in the Analog Module the same, I don't have and image reference for that but I am confident that the connections are correct. The problem is this value doesn't appear always, it's a random value the reading can be 120, 250, 90 degrees and all of a sudden 410. But when I use the second config (32767) the Max value read is 359. If I have a problem with the overflow, how can I correct that? |
7/24/2019 8:07 AM | |
Joined: 5/6/2010 Last visit: 4/30/2024 Posts: 1965 Rating: (272) |
Hello, do you have a overview about the configuration of your sensor? I read at the manual that there are a lot of possible configurations. Can you send a wiring diagram of your application and a specification of your sensor (exactly number. regards |
Follow us on