3/28/2006 1:39 PM | |
Posts: 7 Rating:
|
Hi, I've been trying to use Prodave 6MPI/Ie software but I've noticed that some fuctions are very very slow via mpi bus and some don't work at all via ethernet bus. I've used previos version 5.6 vith several project and I had no problems earlier. When I use db_write (ver 5.6) and db_write_ex6 (ver 6.0) it take at least 100 times more time to write values to PLC (S7-300) with version 6.0 than previous 5.6 version. I wonder what causes that. I have also tried via ethernet and db_write_ex6 allways fails with error 0x410e. Same result when using db_read_ex6. But when I use field_write_ex6 and field_read_ex6, they work fine via mpi and via ethernet. Does anyone else have this kind of problems ?[:o] Attachment_prodave1.pdf (914 Downloads) |
Follow us on