Industry Online Support
Technical Forum
1/8/2008 11:39 AM | |
Posts: 80 Rating: (1) |
Dear All, I try to setup a system using S7 CPU 315-2DP and a Pro-face (GP2501S) screen comm. to CPU via MPI port directly (without adaptor). Then a Ethernet module CP343 attached to the CPU for me to online with CPU via S7. Every time i plug in Pro-face comm. cable to MPI port, the Ethernet connection is interrupted. But Proface comm. is working. I try to change MPI address of CP343 and GP2501S node address, result is still same. I also reduce connection resources for S7 standard comm. at CPU properties 'Communication' tab (Hardware Configuration), and increase OP and PG comm. also still not succesful. Attached is S7 program. anybody have experience about it? thanks in advance regards azad AttachmentProface_.zip (535 Downloads) |
Follow us on