6/29/2011 11:51 AM | |
Posts: 9 Rating:
|
Hi Is there a DTM that i can download for profibus 5613 A2 ? |
6/29/2012 10:56 AM | |
Posts: 21 Rating:
|
Is there seriouly no DTM for the Cp5613? |
6/29/2012 4:34 PM | |
Joined: 9/27/2006 Last visit: 4/18/2025 Posts: 12346 Rating:
|
Hello Shaka; Sorry it took over a year to see your post. Basically yes, you are right, there is no DTM file for a CP 5613 A2. The attachment shows the list of all Siemens DTMs available from the FTD Group (the group that standardizes the DTMs). You can confirm this here: http://www.fdtgroup.org/product-catalog/certified-dtms?company=Siemens+AG&field_device_type_value_many_to_one=All&field_protocol_value_many_to_one=PROFIBUS What exactly were you planning on doing with a DTM for the CP 5613 A2? If you study the list of Siemens DTM-enables slaves, you will notice they are all instruments, setup for Profibus-PA. A CP 5613 A2 is a communication processor for a PC, over Profibus-DP and MPI, for example. Please tell us more on your project. Hope this helps, Daniel Chartier |
7/10/2012 10:06 PM | |
Joined: 9/27/2006 Last visit: 4/18/2025 Posts: 12346 Rating:
|
Hello Shaka; I believe all Softing software is dedicated to Softing harware, but I found this little bit of information from T&H that could offer a glimmer of hope in your case: The Trebing & Himstedt Prozeßautomation GmbH & Co. KG CommDTM PROFIBUS DP-V1 can be used in all FDT frame applications (such as FieldCare or PACTware). It allow communication between PROFIBUS-PA devices, HART devices– connected to the PROFIBUS via Remote I/O (RIO) with HART functionality – and their deviceDTMs. This can be done either centrally through the xEPI 2, or locally (on-site operation in the field) through a PROFIBUS communication processor (CP5512, CP5611 PC card or Field PG with integrated CP5611). http://www.t-h.de/fileadmin/inhalt/IC/downloads/dtm_library/software/User_Manual_CommDTM_PROFIBUS_DP-V1.pdf |
Follow us on