5/23/2014 1:44 PM | |
Joined: 5/12/2014 Last visit: 9/9/2020 Posts: 149 Rating: (16) |
Dear Experts, Up to which distance we can use the profibus cable & Ethernet Cable??
|
5/23/2014 1:55 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello Chetan2490, Profibus Have a Look on the FAQ without Using the Repeator..... Acceptable line length in PROFIBUS-DP networks What should you watch out for when using the RS485 repeater in PROFIBUS and MPI bus systems? if you have more distance than you can used the OLM. Ethernet Its Normally Depend on the Which Cable you are using Cat6 is support up to 50-60 meter. (Approx.) if more Than that, used Optical Convertor. |
Ammy |
|
5/24/2014 8:27 AM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating: (9) |
Nice jpg. .Gives u all the info in single image |
5/24/2014 9:36 AM | |
Joined: 1/21/2013 Last visit: 10/23/2024 Posts: 4620 Rating: (708) |
Hello SMHZ, Go to page 58-401: CPU-CPU communication with SIMATIC controllers - Siemens ...
|
Last edited by: Ste39 at: 5/24/2014 9:47 AM |
|
5/24/2014 10:07 AM |
|
Posts: 784 Rating: (52) |
We are welcome |
5/24/2014 3:18 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, |
VANDE MATARAM..... |
|
Follow us on