6/25/2013 6:38 PM | |
Posts: 8946 Rating:
|
What PLC do you use? Have a look at IM308C what is a often used profibus - device. |
6/25/2013 7:19 PM | |
Joined: 9/27/2006 Last visit: 6/29/2024 Posts: 12264 Rating:
|
Hello Saravana Kumar; I agree with IBN-Service that your best bet Is the IM 308-C, if you can get your hands on a working model. Have a look at the followingdocumentation on the IM 308C and its programming: ET 200 Distributed I/O System with IM 308-C and S5-95U Configuration of the IM 308C DP-masterconfiguration requires Com Profibus software. This manual describes version 3.3, the latest version was 5.1, both versions are quite similar. COM PROFIBUS In the following FAQ you will find several sample configurations with an IM 308C as DP-master with a S7 CPU as slave. This is probably more complex than you need, but it will give you some insights in the setup of the master configuration through COM Profibus. What master/slave communication options are available on PROFIBUS DP? There are also various threads on the forum discussing the connexion of a IM 308C with Siemens drives. Here is one. You would have to adapt it to the requirements of the ABB RPBA Profibus module. communication between s5(IM 308 C) and s120 drive EN / RPBA-01 User's Manual - Abb Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/25/2013 7:21 PM |
|
6/25/2013 7:37 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, Here you can downolad demo version of COM Profibus V3.3 Hope this helps you. |
Last edited by: Amit_86 at: 6/26/2013 5:29 AMLink Corrected VANDE MATARAM..... |
|
6/25/2013 7:49 PM | |
Joined: 11/8/2011 Last visit: 4/12/2024 Posts: 387 Rating:
|
HI AMIT_86 your link directing to web navigator (COM Profibus V3.3) |
This contribution was helpful to
1 thankful Users |
6/25/2013 7:51 PM | |
Joined: 2/6/2009 Last visit: 6/18/2024 Posts: 939 Rating:
|
[quote user="Amit_86"][quote user="Saravana kumar"]hey, where can I get the com profibus software,is it free to download from forum. Hello, Here you can downolad demo version of COM Profibus V3.3 Hope this helps you. Hi, As you mentioned early in your thread the latest version is 5.1. is it ok to use the older version, or can I get latest version? |
_______________________________________________________________ |
|
6/25/2013 7:57 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating:
|
Hello, which PLC? For 95U you need a PLC that support profibus "master". It is not possible to use a additional card. If you need a IM308C contacct me - i have 3UC11 and 3UC21. Regards
André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
6/25/2013 8:04 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating:
|
Hello, then you can use IM308C. But i am not sure that you can use COM Profibus V3. I think you must use V5. Where are you come from? Regards
André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
Follow us on