Industry Online Support
Technical Forum
1/3/2010 12:09 PM | |
Posts: 15 Rating: (0) |
Hi all I am trying to communicate with Magflow 6000 flowmeter over profibus. I have S7400H and am using Y-Link. I imported the GSD file si018129.gsd (profile 3) and tried to go online from HW configuration but it gives the error that the configuration does not match with the slave The flowmeter SW ver is 3.03 and profibus module SW ver is 2.01 rev C. I am sure that the wiring and termination are correct and I can see the node from Profibus diagnostics on my PG. I have also verified the correct IDnumber which is 8192on the flowmeter.The flowmeter is working fine and readings are available locally but I am not able to read or monitorany data at the plc. The attached files show my configuration and the diagnostic data. Am I missing anything? Pls advice at the earliest since i am on site conducting commissioning. Thanks AttachmentMagflow slave configuration and diagnostics.zip (197 Downloads) |
Follow us on