Industry Online Support
Technical Forum
11/28/2013 11:12 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
One example in order to catch the idea -https://www.festo.com/net/SupportPortal/Files/52474/548726g1.pdf |
This contribution was helpful to1 thankful Users |
11/28/2013 2:57 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello AsAPLC, For easy thinking, if you give us the exact code of the actuator, we will seek the solution. |
11/28/2013 3:16 PM | |
Posts: 9 Rating: (0) |
AUMATIC AC 01.1 ACExC 01.1 Profibus DP
|
12/3/2013 10:16 AM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
i am not quite sure, what your question is. after you inserted your IO data with 12 byte in 12 byte out (which address-offset?) you have to compile and load the hardware configuration to you plc. now you can access the data with e.g. L QW 256 (load out word 0, if address offset is 256) or L IW 256 You have also the possibility to define more process images and update them acyclic with UPDAT_PI or UPDAT_PO (SFC 26+SFC 27) some FAQ: Where and when do you need peripheral addressing? |
Best Regards, |
|
Follow us on