11/26/2011 1:48 AM | |
Posts: 23 Rating: (0) |
Hi All, I am trying to configure a Profibus DP link to an ET200S station on an ABB DCS (AC450 as master). To configure it I need to have the user parameter data as a hex string and configuration data as a hex string. All fairly low level configuration. I configured an ACSM1 drive connected by Profibus by configuring it in the Siemens hardware editor first and copying the parameters to the DCS. I tried this with the ET200S but I can't see the user parameters. Any help would be awesome. Attached are some screen shots from my DCS configuration of the ACSM1 drive. AttachmentConfig.zip (234 Downloads) |
11/28/2011 12:07 PM | |
Joined: 10/7/2005 Last visit: 5/21/2024 Posts: 3005 Rating: (1048)
|
Hello paul_wh |
Cheers |
|
This contribution was helpful to1 thankful Users |
11/29/2011 1:40 AM | |
Posts: 23 Rating: (0) |
Awesome That shows me the stuff I need to see. regards Paul |
This contribution was helpful to1 thankful Users |
Follow us on