3/15/2018 8:23 PM | |
Posts: 3 Rating:
|
Greetings, I’m trying to establish a connection between a CM1242-5 and a CP342-5. I’m doing the program both in TIA 14 and STEP7 5.6, this is due to the CPU 314 (314-1AE04-0AB0) available to me not existing in TIA. I’ve set up the Profibus in S7, configured FC1 and FC2 and gotten no errors. I’ve made sure the PROFIBUS network and device ID’s match in both programs as well as the input and output addresses of the slave and the bus parameters. When I download the software in TIA to the PLC, gives me the error: 16# 02:39B3. The BUSF on the CP342-5 blinks as does the Error and DIAG lights in the CM1242-5. Any idea on what I’m doing wrong? In TIA I've tried with and without master without any change in the result. Pictures annexed to help. Anything else you need let me know. Thanks in advance. AttachmentScreenshots.zip (85 Downloads) |
3/16/2018 1:09 PM | |
Joined: 9/27/2006 Last visit: 4/17/2025 Posts: 12346 Rating:
|
Hello Joaquim; Have a look at these documents showing how to configure a CP 342-5 as a master on Profibus-DP. They may clarify some issues:
https://support.industry.siemens.com/cs/af/en/view/18208090
https://support.industry.siemens.com/cs/af/en/view/109744374 Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
Follow us on