Industry Online Support
Technical Forum
9/7/2011 4:55 PM | |
Joined: 4/24/2006 Last visit: 8/13/2024 Posts: 8713 Rating:
|
Dear ghost_, Perhaps the following links might help: Master-slave connection between two CPUs in different projects DP link between CPU 315-2DP (slave) and S7-400 (master) with STEP 7 v5.3 You can change S7-400 to an S7-300 Best regards, Wizard |
9/12/2011 12:47 PM | |
Posts: 1547 Rating:
|
Hello ghost, maybe this application example can help you: http://support.automation.siemens.com/WW/view/en/20987807 Here is explained, which functions you need to establish a connection between master and slave and sending data. If you transfer a bit, you just have to connect this value to a digital output in the slave. You can also look it up in SIMATIC NET Quickstart CD. Greetings, Rated X |
Last edited by: Rated X at: 9/12/2011 1:00 PM |
|
9/13/2011 1:10 PM | |
Posts: 1547 Rating:
|
Hello ghost, you can take a look at Simatic Net Quickstart CD, too: https://www.automation.siemens.com/net-static/Quickstart2009/quickstart012003/html_76/allgemein/allgemein.htm Maybe this will help you further. There is also an example project you can use for your system. You will have to load all the function which are necessary for DP communication. As far as I know you don't need to load a GSD file for these devices. Regards, Rated X |
Follow us on