1/8/2014 6:16 AM | |
Joined: 1/2/2014 Last visit: 5/24/2024 Posts: 142 Rating:
|
Dear Experts,. How to confgiure the ATM 60 encoder for working as a slave under s7 315. Shall I am able to read n write using SFC14/15? I got the GSDfile. While putting it in the Hardware configuration what should I enter n the paramaters? Some hexadecimal values are there to be entered. Have any one configured with simatic manager please help me out. ![]() ![]() the memory mapping of ATM 60 is not understanding to me. I am attatching theProfibus_encoder_connection.pdf
AttachmentProfibus_encoder_connection.pdf (706 Downloads) |
1/8/2014 1:03 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating:
|
Hello, If your CPu is a 315 2dp, there is no need to use FC14/15. Follow the steps as shown in attached document. Pay attention to the profibus speed and adress of your Encoder. Regards, Marcjan AttachmentSick_encoder.pdf (767 Downloads) |
Problem solved? |
|
This contribution was helpful to
1 thankful Users |
3/22/2014 10:08 PM | |
Posts: 13 Rating:
|
I think that use a counter as a divisor or something like that should be fine. I'm not expert, but that is the most inmediate thing I would do using step 7. |
6/15/2019 5:00 PM | |
Joined: 4/14/2010 Last visit: 5/14/2024 Posts: 525 Rating:
|
AttachmentAbsolute Encoder Example.zip (276 Downloads) |
MS |
|
Follow us on