2/23/2021 3:50 PM | |
Joined: 9/27/2006 Last visit: 8/13/2024 Posts: 12277 Rating:
|
Hello Jackcaress; Haïti and Duris-i have the best suggestion since you have a Siemens S7 CPU: examine the contents of the diagnostic buffer, all encountered faults are logged inside. You can also use the Save As.. button in the diagnostic buffer screen, this will generate a.txt file containing the diagnostic messages, including extra information that can be very useful. Post the txt file here if you need additional help. In the meantime, a description of LED statuses for the CP 342-5 can be found in ch. 2 of this manual: https://support.industry.siemens.com/cs/ww/en/view/8773570 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 02/23/2021 15:51:44 |
|
This contribution was helpful to
1 thankful Users |
2/25/2021 9:27 AM | |
Joined: 3/12/2015 Last visit: 7/17/2024 Posts: 533 Rating:
|
Good morning guys , im at the factory now and i have three machines that are linked via profibus one central machine and two identical cnc machines. on the central machine the busf led is flashing and on machine 2 i have the same problem (busf flashing), they told me that on the machine 2 they replaced the CP342.5 module and attached is the diagnostics from that module AttachmentDiagnose.txt (193 Downloads) |
Follow us on