Industry Online Support
Technical Forum
6/9/2012 2:10 PM | |
Joined: 12/20/2008 Last visit: 6/25/2024 Posts: 556 Rating: (236) |
Dear Experts, Please see the attached hardware configuration and online error which I am getting. Both CPU's in the S7400H system are coming to Run mode, however, the bus fault is still blinking and all the IO rack profibus is showing fault. I have checked the cable and connector and the modules, looks ok, but not sure what else to check, please advise. Urgent support would be helpful. If required, I can make available the remote desktop available to view the HW config online. Thanks,
Attachmentfault.zip (75 Downloads) |
6/9/2012 5:08 PM | |
Posts: 947 Rating: (45) |
Hi! You use active bus connector? |
This contribution was helpful to1 thankful Users |
Follow us on