7/22/2011 6:06 AM | |
Joined: 8/25/2006 Last visit: 4/24/2025 Posts: 2214 Rating:
|
Hello. OLM may be used in any Profibus network. Give specifications of your cable or look at the manualto find which cables is suitable for OLM/G11-1300. |
Last edited by: KSN at: 7/22/2011 6:10 AM |
|
7/22/2011 10:56 AM | |
Posts: 100 Rating:
|
Thanks KSN , Attachment120063T01_SMFO.pdf (130 Downloads) |
7/22/2011 2:30 PM | |
Joined: 10/7/2005 Last visit: 4/24/2025 Posts: 3047 Rating:
|
I wouldn't say you "need" multi mode glass fiber, but rather than you can use itwith the OLM-G1x-1300. If you need to cover a large distance though (>10km between OLM's), you'd use the dearer single mode glass fiber (10/125 or 9/125 μm) with the OLM-G1x-1300. As Rated X said that though, chapter 2.1 and 4.1 of the OLM manual will give you all the details on this. |
Cheers |
|
7/26/2011 10:25 AM | |
Posts: 1547 Rating:
|
Hi Walid Elshazly, yes, looks suitable, is singlemode glasfibre, and should at least cover 10km. Regards, Rated X |
7/26/2011 11:38 AM | |
Posts: 100 Rating:
|
Thanks Rated |
Follow us on