Industry Online Support
Technical Forum
3/5/2009 6:03 PM | |
Posts: 6 Rating:
|
/tf/WW/en/Posts/14182 here it has been mentioned that for sinamics series of drives PKW seems to be omitted. My configuration includes a master CPU 416 DP 2 on a simatic 400 station controlling a SINAMICS S120 CU320 via profibus DP. in the HWconfig i am unable to locate any further telegram structures for PKW communication like th eones i find in all simovert or micromaster manuals version 4. i am going wrong somehwere or pKW communication is not enabled for Sinamics S series ? on the same forum i have seen posts regarding use of SFB 58 59 for achieveing acyclic communication but i could not find any specific documentation regarding the same where can i find more information on SFB some people have mentioned using SFC 14 15 is the correct approach. there are examples bys iemens but they have used micromaster series of drives
|
3/5/2009 6:16 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hello Look at Toolbox SINAMICS S120 V1.3 HF1 / S7 Function blocks Hope this will helps. regards |
This contribution was helpful to
5 thankful Users |
Follow us on