Industry Online Support
Technical Forum
1/9/2012 6:03 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating:
|
Hello, Check all the cables and connectors(terminating resistors !) Profibus modules in the CT have good connection to mother board. Do you have all the Fault OB regarding profibus error in your PLC, the PLC stays in run mode? That makes it easy to read in the diagnostic what node is maybe the cause. Best thing to do is get someone with Profibus Analyser to check your network, if it fails that often it must be detected. Here i have a FAQ that could be usefull for you: http://support.automation.siemens.com/WW/view/en/19379085 Regards, Marcjan |
Last edited by: Marcjan at: 1/9/2012 6:09 PMProblem solved? |
|
This contribution was helpful to
1 thankful Users |
Follow us on