11/12/2008 9:13 AM | |
Joined: 4/24/2006 Last visit: 8/15/2024 Posts: 8715 Rating:
|
Dear annupalani, I hope I understand it right. You have two stand alone profibus lines, each containing a master and it's slave's. You want to connect both profibus lines, why don't you use DP/DP coupler: http://support.automation.siemens.com/WW/view/en/18491063 To exchange data between masters. Best regards, Wizard |
11/13/2008 8:19 AM | |
Posts: 26 Rating:
|
Dear Experts Plz. find word doc(ZIP file)attached with the details of architecture with following details. 1)Master Address 2)Slave address 3)Terminator switch position Kindly advice whether the address assignment and position of switch are O.K. THANKS®ARDS PALANI AttachmentProfibus Repeater-Two Segments with Two Masters.zip (608 Downloads) |
Follow us on