Industry Online Support
Technical Forum
5/4/2007 12:14 PM | |
Posts: 26 Rating: (3) |
Hi, I'm quiet sure I configured Starter in theright way. Although the green led of the DP is lighted up on the CU320 and it is possible to connect on the network with the configuration PC. So the network too, seems to be OK. Our DP signal doesn't seem to get through. When we look at Communication Profibus of the Drive object, the speedvalue stay's gray and also the statusword isn't read correctly. ( via attachment screenshot ). Is there a parameter you have to set, to enable Profibus , or get it actif ? Or can't I be online with the CU320 ( via Starter) when the master PLC is (trying ) sending it's speedsetpoint ? Anyway I can't find what I'm doing wrong. I hope someone could help me. PS: I used the GSE - file from the Firmware Card it self, so that shouldn't be the problem. Attachmentscreen.zip (915 Downloads) |
Follow us on