8/25/2019 7:56 AM | |
Posts: 7 Rating:
|
facing issue with PG/PC block monitoring online and downloding slave PLC Configuration details as following Rcoax wireless network consisting 6 Access Points (W 774-1 6GK5774-1FX00-0AA0) And 22 client (W 722-1 6GK1417-5AB10)+ IE/PB Link (6GK1 411-5AB10) Master PLC- CPU 317-2PN/DP Slave- IM151-7 quantity 22 Project Description- EMS ( 22 Moving nodes with PRB) Existing system running on PROFIBUS Master/Slave(with PRB) Configuration for EMS application. We are migrating Profibus Network to Profinet wireless system with using RCoax and IE/PB Link. 11 slave PLC profibus network migrated successfully on wireless profinet. Remaining 11 slave PLC's communicating on Profibus to master. for more details follow the link PLC Backup. Access Point setting- selected wireless configured with IPCF standard setting. Ipcf Cycle time-64ms HW retries-20 using channel-161,153,48,36,157,44 for 6 access points. Master PLC Profinet update time modified with 128ms. getting 100% communication result for master/slave profinet communication but unable to monitoring slave block online and download plc blocks. software- Step7 5.5 sp4 HF11 Please support for setting of profinet to get PG/PC online with slave plc. Thank You. AttachmentPrrofinet NW setting.docx (53 Downloads) |
Follow us on