Industry Online Support
Technical Forum
1/19/2006 11:09 AM | |
Posts: 26 Rating:
|
hello |
1/19/2006 1:52 PM | |
Joined: 8/31/2005 Last visit: 5/16/2024 Posts: 217 Rating:
|
Hello! There are various measurements to get the response time for PROFIBUS and Industrial Ethernet. These times can vary and they are depending on the configuration of your network. Check the following links! Determining the DP response time and the DP bus cycle time for typical configurations on a not clock-synchronized PROFIBUS DP Determining the transfer time for typical configurations in Industrial Ethernet Determining the transfer time for typical configurations in PROFIBUS Communications via Industrial Ethernet between one S7 head-end and multiple S7 substations |
Greetings, Chris |
|
Follow us on