Industry Online Support
Technical Forum
11/14/2013 2:25 PM | |
Posts: 8 Rating: (0) |
Hi All I am working on an installation using a cpu 313c with cp343-1 (343-1EX30-0XE0)and et200s(IM 151-3 PN standard) and a touch panel KTP600 basic color PN. The comms is on profinet,on the main program the fc11 and fc12 blocks are called on fb100 which itself is called in OB1(call FB100,DB100). please see attached the hardware config and fb100. the ET200s is used to monitor a pump station, on the screen we monitor tank levels and the alarms on the pump station. my problem is that there are alarms on the screen which do not go away when I reset on the screen but the screen is displaying the tank levels which tells me it is communicating with the cpu and I do not have the program for the screen(done by external contractor). Thnks in advance Attachment:FB100.jpg (6 Downloads) |
Follow us on