Industry Online Support
Technical Forum
3/7/2024 9:28 PM | |
Joined: 3/7/2024 Last visit: 3/9/2024 Posts: 2 Rating: (0) |
Profinet device name exists multiple times, IRT not possible For my application, I am using a S7-1500 PLC with two Sinamics S210 drives. After downloading the program to the PLC and respective devices, there are two errors: "Profinet device name exists multiple times" and "Error on partner - IRT not possible at this port". I have attached some images to display the diagnostics buffer, I'm not sure how to proceed with fixing the configuration of this application. I would appreciate any pointers that may lead to the solution for this issue. Thank you in advance,
Attachmentpics.zip (284 Downloads) |
Follow us on