2/1/2011 9:59 AM | |
Joined: 10/7/2005 Last visit: 4/17/2025 Posts: 3047 Rating:
|
Hello Twinsen I don't think you are doing anything wrong and am sure Siemens has a good reason to blockthis kind of configuration when the Metadata based IM153-2 DP/PA link isused behind a PN/DP link. What you can do though is to add/configure the IM153-2 DP/PA link via GSD file behind a PN/DP link. The downside is though that you'll now miss out on the userfriendly PA Network configuration and will need to use the GSD tool for it which you can find HERE. I hope this helps |
Cheers |
|
8/8/2019 6:33 PM | |
Joined: 8/3/2017 Last visit: 3/27/2025 Posts: 142 Rating:
|
Hello, any updates on this matter? I´m facing the same situation on my project and i´m struggling to make it work.... |
8/10/2019 4:23 AM | |
Joined: 10/7/2005 Last visit: 4/17/2025 Posts: 3047 Rating:
|
There is, ask Siemens to develop a metadata based solution and make it available as a Hardware support Package download |
Cheers |
|
Follow us on