8/17/2018 7:50 PM | |
Joined: 4/23/2015 Last visit: 6/12/2023 Posts: 168 Rating: (9) |
Dear Colleagues, could you please explain one thing, which is I believe very simple but I still can't clearly get it I have CPU 315-2PN/DP, and I have to connect to it a distributed Profinet IO IM155-6PN HF, where I want to establish fast data exchange, may be even isochronous data exchange, and also I have to connect via Ethernet an HMI, may be SCADA, and let Ethernet be connected into the plant LAN, to have remote VPN access (pls see attached the sketch) In the CPU 315-2PN/DP there are two Ethernet ports onboard, but as soon as I understand this is still one physical network card. My question is: Can I do this way or not? Will IE RT data exchange create disturbances or traffic overload into Ethernet network, and especiially to the plant LAN? Do I have to use embedded Ethernet port for Profinet only and use additional Ethernet module for other Ethernet connections? Thank you. Attachment1.pdf (174 Downloads) |
Last edited by: _Pavel_ at: 8/17/2018 9:39:05 PM |
|
8/20/2018 6:08 PM | |
Joined: 4/23/2015 Last visit: 6/12/2023 Posts: 168 Rating: (9) |
Hello Jay, thank you. Dear Experts, your comments are appreciated. |
10/25/2019 7:19 AM | |
Joined: 4/23/2015 Last visit: 6/12/2023 Posts: 168 Rating: (9) |
Dear All, I don't believe no one knows the answer ) |
Follow us on