10/4/2019 1:28 AM | |
Joined: 9/27/2006 Last visit: 5/28/2024 Posts: 12257 Rating: (2668) |
Hello GBottle; To setup the S7-1200 as a i-device and generating the needed gsdml file (including the data exchange areas of the i-slave configuration) you will have to work on the hardware configuration of the S7-1200, and a dowload (in Stop mode) will be required. https://support.industry.siemens.com/tf//ww/en/posts/gsdml-s71200/185944?page=0&pageSize=10 Hope this helps, |
This contribution was helpful to1 thankful Users |
Follow us on